DUG_EVlink_WH-07

Managing the cable

  • Ensure that the charging connector and charging cable are securely stored between charging sessions.

  • Wrap the charging cable around the EVlink Home Smart’s cable trough.

  • If EVlink Home Smart is installed indoors, protect the connector by covering it with the dust cap.

  • If EVlink Home Smart is installed outdoors, store the connector by plugging it into the socket of the EVlink Home Smart.


QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?