DUG_EVlink_WH-07

Wiser Home AI

Use the Wiser Home app, to view device control and schedules.

The Wiser Home AI feature automatically schedules high energy consumption devices to run during lowest electricity rates, helping in savings on electricity bills. By enrolling devices like EV chargers or resistive water boilers, this feature shifts loads to low-tariff periods. It also helps the EV chargers to consume the excessive solar energy production. It works with variable tariffs, such as peak/off-peak rates, and requires users to answer routine questions.

For more information on Wiser Home AI refer to the respective System User Guide.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?