DUG_EVlink_WH-07

Resetting the PIN using eSetup app

If eSetup PIN code is lost, you can reset the PIN code to default value using the eSetup app.
  1. Power on the EVlink Home Smart to activate the EVlink Home Smart Wi-Fi® direct.
    The Wi-Fi® direct will remain active for 4 minutes after power on.
  2. Open eSetup app and select EVlink Home Smart, and then tap Open Settings.
  3. Select EVlink Home Smart - International or EVlink Home Smart - France based on where the EVlink Home Smart is installed.
  4. On the screen enter the New PIN, confirm the PIN and tap Save.
  5. Tap Reset PIN (A) and select Confirm (B).
  6. Press the Stop button within 3 minutes, 30 seconds.
    NOTE: Unlock the Stop Button by rotating it 90° clockwise.

  7. After 10 seconds, enter the New PIN, confirm the PIN and tap Save.
    NOTE: The PIN must contain 6 to 16 digits, cannot contain the same digit more than 3 times, or a suit of 6 digits or more.
    New PIN update is successful.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?