DUG_Exxact - Blind Control Switch_WH-01

Shutter Calibration without Wiser app

To set the calibration without Wiser app:

  1. Press bottom and top push-buttons for 3 seconds.
    The status LED blinks green.
    • If the shutter is not in a completely open position, it starts to open and reaches the top position.

    • In this step, If the shutter is already in the open position, then there will be no movement of the shutter.

    NOTE: LED blinks green throughout the calibration process.
  2. Short press the top push-button when the shutter opens completely.
    The shutter starts to close and reaches the bottom position.
  3. When the shutter reaches the bottom position, immediately press the top push-button once.
    The shutter starts to open and reaches the top position.
  4. When the shutter reaches the top position, immediately press the top push-button once.
    Shutter starts to move and automatically reaches a middle position to finish the calibration.
    NOTE: The exact shutter position depends on the shutter type, motor and mechanical construction. Based on this, the middle position will differ.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.