DUG_Exxact - Blind Control Switch_WH-01

Editing an automation

Follow the steps to edit an automation:
  1. On the Home screen, tap .
  2. Go to Automation, tap the automation you want to edit (A).
  3. On the Edit automation page, you can:
    • Change the icon.
    • Rename the automation.
    • Change the condition or action.
  4. Remove the Condition or Action by swiping it to the left and tapping the bin icon (B).
  5. Add a new condition or action and then tap Save.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?