DUG_Exxact - Blind Control Switch_WH-01

Identifying the device

Using the Wiser Home app, identify the blind control switch among the devices available in a home.
  1. On the Home screen, tap .
  2. Tap Devices > Shutters > Blind control switch or Shutter slat > Identify (A).
    The status LED blinks red and the shutter opens/closes gradually, upon successful identification of the blind control switch or shutter slat.
  3. Tap OK to finish identifying the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?