DUG_Exxact - Blind Control Switch_WH-01

Selecting the device location

Using the Wiser Home app, you can add the blind control switch to any room (such as living room, bedroom, kitchen etc).
  1. On the Home screen, tap .
  2. Tap Devices > Shutters > Blind control switch or Shutter slat > Location (A) to assign the blind control switch to an existing room or a new room (B) and tap Submit.
    TIP: You can also select a device from the list in the Control tab, tap > Device Settings.
    NOTE:
    • If the device is already assigned, you can remove it from the existing room by tapping Remove from Room.

    • Blind control switch is the name given to the device when pairing with the Wiser Hub. You can assign a name according to your shutter type. Example, Shutter slat.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?