DUG_Exxact - Termostaatti 16 A ZB_WH-00

Cancel all overrides

The Cancel all overrides (A) will put all the heating back under ‘system control’ meaning that if you’ve selected Boost All or even if you’ve boosted or manually overridden a room setpoint individually, this will cancel the override and put all the rooms back to their scheduled set points. You can find it in the “Automation” menu by tapping the “Automation” tab at the bottom of the Home screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Auttoiko tämä?