Troubleshooting
|
Symptom |
Possible cause |
Solution |
|---|---|---|
| Device Error | Try reinstalling the device. If the error persists, replace the device. | |
|
Individual PowerTag data is not available in home screen. |
|
Restart the device. Also, ensure to correct the Ethernet connection. |
|
The hourly data is incorrect against real local time. |
Incorrect time configuration as per the user’s country. |
Set correct time zone as per your country. |
|
The LED of PowerTag is blinking amber. |
PowerTag not yet commissioned to the hub for the first time. |
Commission the PowerTag to the hub. Refer to Pairing the device. |
|
PowerTag is out of range from Hub. |
Perform any of the methods:
|
|
|
The LED of PowerTag blinks red rapidly. |
PowerTag is out of range from Hub. |
Perform any of the methods:
NOTE: If the LED still blinks red, replace with a new device
and try adding again.
|
|
Hub is powered down |
Power ON the Hub. |
|
|
The LED of PowerTag is glowing red permanently. |
The device is not working permanently. |
Replace with a new device and try adding again. |
|
The LED of PowerTag is OFF |
PowerTag is probably not powered ON. |
Recheck the wiring and power connection of the PowerTag and see if gets powered ON. Try adding the device after it is powered ON. If the above mentioned method do not work, replace the PowerTag and retry. |