DUG_SysM/SysD SSO 16 A_WH-07

About the device

The Connected Single Socket Outlet 16 A (hereinafter referred to as a Socket outlet) is a connected electrical outlet designed to manage and control electrical devices in a convenient and efficient manner.

The Socket outlet is equipped with:

  • Temperature protection mechanism: When the Socket outlet is used with a high load over a long time, the mechanism can switch off the Socket outlet, ensuring overheat protection.

  • Overload protection mechanism: When the Socket outlet is used with a high load (~18A or higher), the mechanism can switch off the Socket outlet, ensuring overload protection.

Features of a Socket outlet:

  • Remote access: You can switch On/Off the Socket outlet using the app or through a connected wireless switch or through voice control (Google Home, Amazon Alexa, Siri) in addition to using the On/Off button on the device itself.

  • Power consumption: You can monitor power (W) consumption using the app.

  • Easy installation: The Socket Outlet fits in existing wall boxes (40 mm), no separate wall box requirement.

  • Easy scheduling: You can create a schedule for the various device functions in an easy manner as per your specific requirements for comfort and convenience.

  • High safety: The integrated overload and overheat protection ensures that the Socket outlet is safe at all times.

NOTE:
  • The device must not control safety-relevant applications

  • Do not mix different load types in the controlled socket

  • Do not use multi-sockets in the controlled socket

  • Do not use for EV charging

Diagram of operating element

  1. Push button with status LED

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?