DUG_SysM/SysD SSO 16 A_WH-07

LED indications

Pairing the device

User Action

LED Indication

Status

Press the push button 3 times

LED blinks amber, once per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a time, before turning Off.

Resetting the device

User Action

LED Indication

Status

Press the push button 3 times and hold it down once for > 10 s.

After 10 s, the LED starts blinking red.

The device is in reset mode. It is reset to the factory settings after 10 seconds. The device then restarts, and the LED glows solid orange.

Setting (Default state)

Status

LED Indication

Description

The Red LED glows.

The Red LED glows when the output is switched ON.

All the LEDs are OFF.

The LEDs are OFF, when the output is OFF.

Alarms

Status

LED Indication

Description

Blinking red fast

When there is an overload or over temperature alarm and the device is switched off.

LED Indicator Mode/Backlight Mode

Load Status

ON

OFF

Reverse with load

No LED

Consistent with load

No LED

Always Off

No LED

No LED

Always On

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?