DUG_Unica-Wireless Switch_WH-05

Assigning a Moment to the Wireless switch

A Moment allows you to group multiple actions that are usually done together. You can configure a Moment to the Wireless switch (such as Good Night Moment: Fan on, light dimming 50%, shutter close).
TIP: A moment can be assigned to any of the four keys individually.

To configure a Moment to the Wireless switch:

  1. On the Control tab, tap All devices or the room tab where the Wireless switch is located.

  2. Tap any key and select Moment.

  3. Select a Moment which you want to add to the key and tap Select Moment.

    In the next screen, shows the Moment is successfully configured.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?