DUG_Unica-Wireless Switch_WH-05

LED indications

Pairing the device

User Action

LED Indication

Status

Press the push button 3 times.

LED blinks orange, once per second.

Pairing mode is active for 30 seconds. When pairing is completed, LED displays solid green for a few seconds, before turning Off.

Resetting the device

User Action

LED Indication

Status

Press the push button 3 times and hold it down once for > 10 s.

LED blinks red, once per second.

The device is in reset mode. The device then restarts and the LED starts blinking green, before turning Off.

Battery level

LED Indication

Status

LED blinks red once, when a push button is pressed.

The battery is low (< 10%). Replace the Wireless Switch battery.

NOTE: A notification pop-up will appear on the app.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?