DUG_Unica-Wireless Switch_WH-05

Assigning an Action to the Wireless switch

You can configure an Action to the Wireless switch (such as turning on/off the lights, moving the shutter up or down or any combination).

To configure an Action to the Wireless switch:

  1. On the Control tab, tap All devices or the room tab where the Wireless switch is located.

  2. Tap any key and select Action.

  3. Select the device and tap Select Action.

  4. On the Configure Device screen, select the Light Switch.

  5. Tap to turn on the light and tap Set > Set Action.

    In the next screen, shows that the Action is successfully configured.

    The Top Left key is configured with Light Switch: On.

    TIP: When assigning a push button to control a dimmer or a shutter, it is important to know that you can set a specific percentage for brightness or shutter position. For example, if you configure a dimmer to 50%, short pressing the push button will turn on the light directly at 50% brightness. Similarly, for shutters, you can set a position to 30% open. When you short press the push button, the shutter will automatically move to that position.
    NOTE: Pressing and holding the push button cannot dim the light or open/close the shutter. Only short press actions are supported in the Wireless switch.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?