System User Guide Wiser Home (France) - 14

Hubs

The Hub monitors and controls the Devices of your Home via the Wiser Home app, using Wi-Fi®.

Wiser HubR 2nd Generation

CCTFR6311G2

The Wiser HubR is used to connect all the Wiser devices. This version is used where central heating (e.g. boiler or heat pump) is used.

Instruction Sheet (PDF)

Getting to know the Hub

Wiser Hub 2nd Generation

CCT501801

The Wiser Hub 2nd Generation monitors and controls the Devices of your Home via the Wiser Home App. It is connected to the Wiser Cloud for remote control via Wi-Fi®.

The Wiser Wiser Hub 2nd Generation is compatible with all Wiser Devices

Instruction Sheet (PDF)

Getting to know the Hub

Wiser Wall Box Power Supply

CCT501800-0001

Alternative power supply for the Wiser Hub 2nd Generation, placed in a wall box.

Instruction Sheet (PDF)

Wiser HubR

CCTFR6311

The Wiser HubR is used to connect all the Wiser devices. This version is used where central heating (e.g. boiler or heat pump) is used.

NOTE: Certain Wiser Devices can not be added to the Hub.

Check the Device compatibility list.

Instruction Sheet (PDF)

System User Guide

Wiser Hub

CCTFR6310

The Wiser Hub is used to connect and control all the Wiser devices.

NOTE: Certain Wiser Devices can not be added to the Hub.

Check the Device compatibility list.

Instruction Sheet (PDF)

System User Guide

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.