System User Guide Wiser Home (France) - 14

Energy Domain with Grid

If you have an energy device installed, like a PowerTag E, the Energy Centre will be available.

In the Energy Centre, you can monitor your energy consumption and production, view detailed history, and get information on energy savings.

IMPORTANT: The Wiser system supports the configuration with the following power source combinations where PowerTag Energy sensors are installed.
  • Grid

  • Grid and Solar

  • Grid and Solar, and Battery and Solar (combo)

    .

To navigate to the Energy Centre:

  1. Tap .

NOTE: If you do not have any energy devices installed, like a PowerTag E, Insights will be displayed.
NOTE: You can find the detailed information in the Device User Guide of the respective device.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.