DUG_Motion Sensor_WH-05

Setting device notification

Using the Wiser Home app, you can enable or disable the sensor notification.
  1. On the Home screen, tap .
  2. Tap Devices > Motion Sensor > Notify me if motion detected (A) to enable or disable the sensor notification toggle switch.
    TIP: Additionally, you can enable or disable the sensor notification toggle switch by tapping on the Control tab Motion Sensor > Device settings > Notify me if motion detected (A).
    NOTE:
    • Sensor notification toggle switch (A) is OFF by default.

    • Notifications created via automation are treated as separate notifications.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?