DUG_Motion Sensor_WH-05

Removing the device

Using the Wiser Home app, you can remove the sensor from the Wiser system.
  1. On the Home screen, tap .
  2. Tap Devices > Motion Sensor > Delete (A).
    TIP: Additionally, you can remove the sensor from the Wiser system by tapping on the Control tab Motion Sensor > Device settings > Delete (A) .
  3. Read the confirmation message and tap Ok to remove the sensor from the Wiser system.
    NOTE:
    • Removing the sensor will reset the sensor. After resetting, the LED blinks amber indicating that the sensor is ready for pairing.

    • If there is a problem while pairing or resetting the sensor, refer to Resetting the device, Resetting the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?