DUG_Motion Sensor_WH-05

About the device

The Wiser Motion Sensor (hereinafter referred to as sensor) detects nearby movement and measures the luminance of the environment.

The sensor sends the data to the Wiser Hub. The threshold of luminance settings and/or detection of movement can be configured in the Wiser app.

Features of the sensor:

  • Detect motion and send this information to the Wiser Hub.

  • Detect and measure the lux level of the environment and passes the information to the Wiser Hub.

  • Sends the sensor battery level and offline status information to the Wiser Hub.

Operating elements

  1. Function key

  2. Status LED

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?