DUG_Motion Sensor_WH-05

Checking the device history

Using the Wiser Home app, you can view the sensor history, which provides information about when motion detected event was logged. Each motion detected event is logged and stored in the cloud.
NOTE: If the cloud connection is lost, the motion events will not appear in the history.
  1. On the Control tab, tap All devices or a room tab where the sensor is located.
  2. On the device control panel page, tap History.
    TIP: The logged event appears on the history page, even if the motion notification switch is toggled off on the device details page.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?