DUG_Motion Sensor_WH-05

Using the device

The Control Panel of the sensor allows you to view if the motion is detected or not.
  1. On the Control tab, tap All devices or a room tab where the sensor is located.

  2. On the Sensor control panel page, you can see the following:

    • Current lux level (A)

    • Motion detection status (B)

    • History (C)

    • Device settings (D)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?