Pairing the device with the Wiser HubR
- On the Home screen, tap
.
- Tap icon and tap Climate > Room Thermostat.
- Tap Scan QR code and allow the Wiser
Home app to access your camera. Then, scan the QR code located on
the device.NOTE: If you are unable to find the correct QR code, tap I can't find the correct QR code to pair the device manually and proceed to step 4.
If the QR code is incorrect, a message Incorrect QR code scanned will appear. Tap I can't scan the QR code and choose one of the following options:
-
(A): Enter the Mac Address/EUI-64 and Install Code, then tap Connect. The app will verify if the Mac Address/EUI-64 and Install code are valid.
-
(B): Tap this option if you are unable to find the Mac Address/EUI-64 and Install code.
-
- Tap Next to enter Room Thermostat name and assign it to an existing room or a new room, then tap Submit.
- Tap Heating Type and select one
of the following and tap Done:
- None: In case Underfloor Heating (UFH) hasn't been installed or if you prefer not to use a room thermostat with UFH, select None and proceed to Step 7.
- Underfloor Heating: If Underfloor Heating is installed and you wish to use room thermostat along with UFH, select Underfloor Heating and proceed to Step 6.
- Update following details:
- UFH Channels: Select the channel which is assigned to the same room as room thermostat in Step 4.
- Assign Floor Sensor: Turn on the toggle switch if you want to use the UFH floor sensor which is assigned to the same room as room thermostat.
NOTE:-
To change the UFH channel room refer Assigning a channel to the room.
-
Only one UFH floor sensor can be assigned to a room if you want to update refer Setting Floor Sensor Location.
- Tap Submit to complete the pairing process.
The Room Thermostat is now listed on the Control tab under the All and the specific room tabs.