DUG_Room Thermostat_WH-09

Setting room temperature manually

You can increase or decrease or boost the room temperature using the Room Thermostat button.

The room temperature can be increased or decreased, and boost time can be set using a Room Thermostat button.

  • Press the + button to increase the set-point temperature by 0.5 °C.

  • Press the - button to decrease the set-point temperature by 0.5 °C.

NOTE: After each set point change, wait 10 seconds and check that the desired set point is being displayed.

The amount of time the boost remains active depends on how many times you press O as follows:

  • Press 1 time = 30 minutes

  • Press 2 time = 1 hour

  • Press 3 time = 2 hours

  • Press 4 time = 3 hours

  • Press 5 times = Cancel

NOTE: With only boost features, you can set the time like how long you want the room to be heated up.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?