DUG_Window/Door Sensor_WH-06

Using the device

The Control Panel of the sensor allows you to view if the window/door is opened or closed.
  1. On the Control tab, tap All devices or a room tab where the sensor is located.

  2. On the sensor control panel page, you can see the following:

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?