DUG_Window/Door Sensor_WH-06

Identifying the device

Using the Wiser Home app, you can identify the sensor from the other available devices in the room.
  1. On the Home screen, tap .
    NOTE: Please wake up the sensor (press the function key).
  2. Tap Devices > Window/Door Sensor > Identify (A).
    TIP: Additionally, you can identify the sensor by tapping on the Control tab Window/Door Sensor > Device settings > Identify (A).
    NOTE: The sensor LED blinks to identify the sensor and it continues blinking green until you tap OK.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?