DUG_Window/Door Sensor_WH-06

Resetting the device

You can reset the sensor to factory default manually.
To reset the sensor:
  1. Remove the primary part from the base plate by sliding it upwards.
  2. Short-press the function key 3 times (<0.5 s) and then long-press the function key once (>10 s), the LED blinks red after 10 s, and then release the function key.
    Upon successful reset of the sensor, the LED stops blinking. Then, the sensor restarts and blinks green for a few seconds.
    NOTE: After reset, the LED turns off to save the battery.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?