DUG_Window/Door Sensor_WH-06

Removing the device

Using the Wiser Home app, you can remove the sensor from the Wiser system.
  1. On the Home screen, tap icon.
  2. Tap Devices > Window/Door Sensor > Delete (A).
    TIP: Additionally, you can remove the Sensor from the Wiser system by tapping on the Control tab Window/Door Sensor > Device settings > Delete (A).
  3. Read the confirmation message and tap Ok to remove the sensor from Wiser system on the next screen.
    NOTE:
    • Removing the sensor will reset the sensor. After resetting, the LED blinks amber indicating that the sensor is ready for pairing.

    • If there is a problem while pairing or resetting the sensor, refer to Resetting the device.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?