DUG_Window/Door Sensor_WH-06

Example of an automation

This demonstration shows you how to create an automation to turn on the light switch when the Door is open during Night time.
  1. Go to Automation > to create an automation.
  2. To add a condition, tap Add Condition > Device status change > Door Sensor, tap (A) to Open, then tap Set.
  3. Read the information and tap OK.
  4. To set the time, tap When > Add time > Period of time > Night time > Set.
  5. To add an action, tap Then > Add an action > Control a device > Micromodule Switch, tap (B) to turn on, then tap Set.
  6. Read the information and tap OK.
  7. Enter the name of the automation.
    TIP: You can choose the cover image that represents your automation by tapping .
  8. Tap Save.
    Once the automation is saved, it is visible on the Automation tab.
    NOTE: You can enable or disable automations on the Automation tab by using (C).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?