80043-870-01

Installation

DANGER
hazard of electric shock, explosion, or arc flash
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices. See NFPA 70E, CSA Z462, or NOM-029-STPS.
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn OFF all power supplying this equipment before working on or inside the equipment.
  • Always use a properly rated voltage sensing device to confirm power is OFF.
  • Read and understand this entire instruction bulletin and the included NEMA PB 1.1 standards publication before installing, operating, or maintaining this equipment.
  • Local codes vary, but are adopted and enforced to promote safe electrical installations. A permit may be needed to do electrical work, and some codes may require an inspection of the electrical work.
  • Replace all devices, doors and covers before turning ON power to this equipment.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?