Introduction
This bulletin explains how to install the Powerlink™ G4 Remote Mount Controller, which is used to control the operation of a Powerlink G4 system. Refer to Remote Mount Controller Part Numbers in the Appendix for controller system voltages and catalog part numbers.
The Remote Mount Controller and power supply is factory mounted in a NEMA Type 1 enclosure.
The Powerlink G4 controller uses remotely operated circuit breakers to control up to 168 remotely operated branch circuits. Control signals originate externally from dry-contact inputs, from the internal time scheduler, or from commands received via the communications network. Typical control devices include low voltage push button wall switches, occupancy sensors, photocell controllers, and security and building management systems. Refer to Technical Specifications in the Appendix for controller specifications.
For more information on installing and operating Powerlink G4 Controllers refer to the appropriate Powerlink G4 Controller instruction manual. See Powerlink Instruction Manuals in the Appendix.