80043-870-01

Operation

After all connections are made and all covers are in place:

  1. Energize the Remote Mount Controller by turning on the circuit breaker feeding power to the power supply.

  2. Verify that the power supply is installed correctly. If the CL1 and CL2 LEDs are lit (Power supply LEDs), the power supply is connected properly.

    Power supply LEDs


  3. Verify that the controller is installed correctly. If the LCD screen of the controller displays information, then the controller is operating (Controller LCD screen).

    Controller LCD screen

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?