80043-870-01

Reinstalling the Trim Front

Reinstall the trim front using the screws retained when removing the trim front, see (Reinstalling the trim front).

Reinstalling the trim front

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?