Prepare Database and Create Domains
Prepare your database
Right-click your database in ArcCatalog and run both of the following tools:
Create Domains
Apply the following domain properties to each domain listed below.
- Field Type: Long Integer
- Domain Type: Coded Values
- Split policy: Duplicate
- Merge policy: Default Value
FdrMgrNonTraceable
If you plan to create a FdrMgrNonTraceable field on one or more of your edge feature classes, create a domain to be applied to fields carrying the FDRMGRNONTRACEABLE field model name (assigned in a future step).
|
Code |
Description |
|
0 |
Traceable |
|
1 |
NonTraceable |
NormalStatus
This domain provides values for the possible positions of switchable devices.
|
Code |
Description |
|
0 |
Open |
|
1 |
Closed |
|
2 |
Not Applicable |
Phase Designation
Phasing allows you to maintain information on individual phases of a conductor or device.
|
Code |
Description |
|
1 |
C |
|
2 |
B |
|
3 |
BC |
|
4 |
A |
|
5 |
AC |
|
6 |
AB |
|
7 |
ABC |
Single Phase
This domain provides phasing for single-phase conductors and devices.
|
Code |
Description |
|
1 |
C |
|
2 |
B |
|
4 |
A |
Two Phase
This domain provides phasing for two-phase conductors and devices.
|
Code |
Description |
|
3 |
BC |
|
5 |
AC |
|
6 |
AB |
Three Phase
This domain provides phasing for three-phase conductors and devices.
|
Code |
Description |
|
7 |
ABC |
Transformer Unit kVA
The ArcFM Electric Trace Options includes an option to display kVA by phase for a trace. To access this option in ArcMap, click the Options button on the ArcFM Electric Traces toolbar and select the Electric Traces tab:

With this option checked, the Rated kVA dialog is shown after each trace. This displays the sum of the Rated kVA (by phase) for all transformer units returned by the trace. If transformer units are not present, the rated kVA is calculated from the kVA values of the transformers. If it's not configured, or configured incorrectly, it displays values of 0.0.

To display Rated kVA for a trace, you must create the following domain. This domain holds the possible Rated kVA values in your network. The following table shows an example of how you might create this domain. Your domain will probably have more values.
|
Code |
Description |
|
10 |
10 kVA |
|
15 |
15 kVA |
|
25 |
25 kVA |
|
38 |
37.5 kVA |
|
50 |
50 kVA |
|
75 |
75 kVA |
|
100 |
100 kVA |
YesNo
This domain is used for numerous fields across the ArcFM Solution.
|
Code |
Description |
|
0 |
No |
|
1 |
Yes |
Create Model Name Domains
If they do not already exist, create and populate the domains that contain the electric field and object class model names. Apply the following domain properties to each domain listed below.
Field Type: Text
Domain Type: Coded Values
Split policy: Default Value
Merge policy: Default Value
Electric Field Model Name
Populate this domain with all of the following field model names.
|
Code |
Description |
|
CIRCUITSOURCEID |
CIRCUITSOURCEID |
|
FDRMGRGANGOPERATED |
FDRMGRGANGOPERATED |
|
FDRMGRNONTRACEABLE |
FDRMGRNONTRACEABLE |
|
FACILITYID |
FACILITYID |
|
FEEDERID |
FEEDERID |
|
FEEDERLEVEL |
FEEDERLEVEL |
|
FEEDERNAME |
FEEDERNAME |
|
LOWSIDEVOLTAGE |
LOWSIDEVOLTAGE |
|
MMELECTRICTRACEWEIGHT |
MMELECTRICTRACEWEIGHT |
|
NORMALPOSITION_A |
NORMALPOSITION_A |
|
NORMALPOSITION_B |
NORMALPOSITION_B |
|
NORMALPOSITION_C |
NORMALPOSITION_C |
|
OPERATINGVOLTAGE |
OPERATINGVOLTAGE |
|
PHASEDESIGNATION |
PHASEDESIGNATION |
|
RATEDKVA |
RATEDKVA |
|
SUBSOURCE |
SUBSOURCE |
|
SUBSTATIONID |
SUBSTATIONID |
Electric Object Class Model Name
Populate this domain with all of the following object class model names.
|
Code |
Description |
|
CIRCUITSOURCE |
CIRCUITSOURCE |
|
CIRCUITSOURCEID |
CIRCUITSOURCEID |
|
DYNAMICPROTECTIVEDEVICE |
DYNAMICPROTECTIVEDEVICE |
|
ELECTRICNETWORKEDGE |
ELECTRICNETWORKEDGE |
|
FDRMGRLOADPOINT |
FDRMGRLOADPOINT |
|
FDRMGRNONTRACEABLE |
FDRMGRNONTRACEABLE |
|
FDRMGRPROTECTIVE |
FDRMGRPROTECTIVE |
|
FEEDERSECONDARY |
FEEDERSECONDARY |
|
OPENPOINT |
OPENPOINT |
|
PROTECTIVE |
PROTECTIVE |
|
SPLITTARGET |
SPLITTARGET |
|
SWITCH |
SWITCH |
|
TRANSFORMER |
TRANSFORMER |
|
TRANSFORMERUNIT |
TRANSFORMERUNIT |