Create Feature Classes
Decide which feature classes to include in your network. Below are the feature classes that Schneider Electric recommends you include in your geodatabase. These feature classes are from the Minerville sample geodatabase. You may use different feature class names and include additional feature classes. Throughout this documentation, we will refer to the feature classes as named below.
FdrMgrNonTraceable
The FDRMGRNONTRACEABLE model name may be assigned to a feature class or to an attribute field. If it is assigned at the feature class level, the entire class will be omitted from Feeder Manager 2.0 traces.
You may also create a Feeder Manager NonTraceable Indicator field to which the model name is assigned. Below are the required data type and domain for this field. You may change the name of the field, but the FDRMGRNONTRACEABLE field model name assigned later must have the EXACT spelling.
|
Field |
Data Type |
Domain |
|
Feeder Manager NonTraceble Indicator |
Long integer |
FdrMgrNonTraceable |
The user will be able to select Traceable or NonTraceable for individual features.
Adetailed explanation of the relationship between FDRMGRNONTRACEABLE and Bitgate values is in the Appendix.
See the help topic Electric Tracing - Edges.
Conductors
Conductors consist of primary and secondary wire as well as other current-carrying lines such as bus and transmission lines. These feature classes must participate in your geometric network as simple edges or complex edges. If you have edges in your network that you don't want Feeder Manager 2.0 to trace (but want to trace them for other purposes, such as bus in a substation that is upstream of the circuit breaker), include these feature classes in your network and use the model name FDRMGRNONTRACEABLE as an object class model name or field model name to disable edge feature classes from the trace. If you want Feeder Manager 2.0 to trace with respect to conductor phasing, you must create a PhaseDesignation field for the edge features in your network. The PhaseDesignation field should be assigned a domain.
Below is a list of required fields for this feature class. You may change the names of the fields, but the field model names assigned later must have the EXACT spelling. Ensure the domains are assigned as shown.
|
Field |
Data Type |
Domain |
|
ElectricTraceWeight |
long integer (precision = 10) |
|
|
PhaseDesignation |
long integer |
On the Properties Subtypes tab, assign the appropriate domain for each subtype: Phase Designation, Single Phase, Two Phase, or Three Phase. |
|
OperatingVoltage |
long integer, domain required |
OperatingVoltage |
|
FdrMgrNonTraceable (optional) |
long integer or string/text |
FdrMgrNonTraceable |
|
FacilityID |
text (length=20) |
Default value = null |
Switchable Devices
Switches can interrupt the flow of electricity in a circuit. You can include non-mechanical open points in this category as well because a switch that is normally open appears the same to the tracing algorithms as an open point. Modeling an open point as a switch allows you to close it out in the field and reflect that change by changing the normal open status fields. You can have one or more feature classes that store switchable devices but each must be assigned the model name of SWITCH. In your model, the switch classes must be a simple junction, and must have fields assigned the following model names. If you want to use the out-of-the-box autoupdaters to maintain the trace weights, the fields carrying the NORMALPOSITION_A, NORMALPOSITION _B, or NORMALPOSITION _C model name should have a domain assigned.
Below is a list of required fields for this feature class. You may change the names of the fields, but the field model names assigned later must have the EXACT spelling. Ensure the domains are assigned as shown.
|
Field |
Data Type |
Domain |
|
GangOperated |
text |
Yes/No |
|
ElectricTraceWeight |
long integer (precision = 10) |
|
|
PhaseDesignation |
long integer |
On the Properties Subtypes tab, assign the appropriate domain for each subtype: Phase Designation, Single Phase, Two Phase, or Three Phase. |
|
NormalPosition_A |
long integer |
NormalStatus |
|
NormalPosition_B |
long integer |
NormalStatus |
|
NormalPosition_C |
long integer |
NormalStatus |
|
CircuitSourceID |
long integer |
|
|
Subsource |
short integer |
Yes/No domain |
|
FacilityID |
text (length=20) |
Default value = null |
Protective Devices
Protective Devices provide overcurrent protection and can interrupt the flow of electricity in a circuit. You can have one or more feature classes that represent protective devices but each must be assigned the model name of FDRMGRPROTECTIVE to designate it as a member of this category. Please note that Feeder Manager 2.0 makes no distinction between the categories of Switchable and Protective Devices. The autoupdaters provided with Feeder Manager 2.0 use the FDRMGRPROTECTIVE model name to maintain the value in the trace weight field. The design of Feeder Manager 2.0 anticipates that future applications (especially outage management) will need to determine from the trace weight alone whether a device is protective or not, i.e., whether it is designed to open automatically in response to a fault. Assign a domain to the fields with model names NORMALPOSITION_A, NORMALPOSITION _B, and NORMALPOSITION_C.
Below is a list of required fields for this feature class. You may change the names of the fields, but the field model names assigned later must have the EXACT spelling. Ensure the domains are assigned as shown.
|
Field |
Data Type |
Domain |
|
ElectricTraceWeight |
long integer (precision = 10) |
|
|
GangOperated |
text |
Yes/No |
|
PhaseDesignation |
long integer |
On the Properties Subtypes tab, assign the appropriate domain for each subtype: Phase Designation, Single Phase, Two Phase, or Three Phase. |
|
NormalPosition_A |
long integer |
NormalStatus |
|
NormalPosition_B |
long integer |
NormalStatus |
|
NormalPosition_C |
long integer |
NormalStatus |
|
CircuitSourceID |
long integer |
|
|
Subsource |
short integer |
Yes/No domain |
|
FacilityID |
text (length=20) |
Default value = null |
Transformers
Transformers are devices that transform the voltage level in a circuit. Transformers must be a junction feature class in your geometric network. You can include Step Transformers in this category as well. This feature class must be assigned the class model name of TRANSFORMER. The Phase Designation field should store the phase or phases that the transformer is tapping and have a domain assigned to it. This enables Feeder Manager 2.0 to determine which phase of a three-phase conductor a single-phase transformer is tapping.
Below is a list of required fields for this feature class. You may change the names of the fields, but the field model names assigned later must have the EXACT spelling. Ensure the domains are assigned as shown.
|
Field |
Data Type |
Domain |
|
ElectricTraceWeight |
long integer (precision = 10) |
|
|
PhaseDesignation |
long integer |
On the Properties Subtypes tab, assign the appropriate domain for each subtype: Phase Designation, Single Phase, Two Phase, or Three Phase. |
|
Optional: Create the following field if you want to display the Total RatedkVA for an electric trace. This functionality also requires the TransformerUnit object class. |
||
|
RatedkVA |
long integer |
Transformer Unit kVA |
|
Optional: Create the following field if you want secondary conductors downstream of a transformer to inherit the transformer's LowSideVoltage value. If this value doesn't exist (and the functionality is configured), the downstream secondary conductors inherit the OperatingVoltage value from the transformer. |
||
|
LowSideVoltage |
long integer |
|
|
CircuitSourceID |
long integer |
|
|
Subsource |
short integer |
Yes/No domain |
|
FacilityID |
text (length=20) |
Default value = null |
CircuitSourceID Object Class
This table stores data about the multi-tiered network.
|
Field |
Data Type |
Domain |
|
FeederLevel |
long integer |
|
|
FeederName |
text (length=48) |
|
|
ObjectID |
Object ID |
TransformerUnit Object Class
|
Field |
Data Type |
Domain |
|
RatedkVA |
Long integer |
Transformer Unit KVA |