Using the Feeder Sync Tool When Posting (Default Configuration)
- In ArcCatalog, right-click your Electric Geometric Network and select Configure Feeder Manager.
- From the Feeder Manager configuration window:
-
Clear the Feeder Manager 1.0 option (if enabled).
-
Select the Feeder Manager 2.0 option.
-
Expand the Advanced Configuration options. Select the Feeder Manager 1.0/Feeder Manager 2.0 Field Sync option.
-
Optionally set the Enable autoupdaters during field sync option to allow autoupdaters to fire during field synchronization.
-
Set the Target version for sync (SDE.DEFAULT by default).

-
- Click OK.
- Create or open a session or design in ArcMap.
- Perform typical editing operations (create/delete features,
editing existing features, etc.) in that session or design.
-
Notice that the Feeder Information fields from Feeder Manager 2.0 update after each edit (Feeder IDs, Subfeeder IDs (if applicable), Energized Phases, Number of Feeders, Loop, Tie Device).
-
Notice that the feeder information in the legacy fields (FeederID, FeederID2, and FeederInfo) do not update after each edit.
-
- Save the session or design. This will populate the MM_EDITED_FEATURES
table.
-
You can add the MM_Edited_Features table to inspect its contents if necessary.
-
- Post the session or design to SDE.DEFAULT. The former Feeder Manager 1.0 fields now populate with the new feeder information (FeederID, FeederID2, and FeederInfo).