Extended Data Definition Tables
Designer’s sample data is installed with several Extended Data Definition (EDD) tables. These tables are Esri objects. If they have been converted to ArcFM or Designer Objects, use the ArcFM Solution Object Converter to convert them back to Esri objects. It is recommended that EDD tables remain unversioned.
EDM_COMPATIBLEUNIT
This table manages the extended data for a compatible unit. No field model names exist. This table has four subtypes:
|
Subtype |
Code |
|---|---|
|
Electric |
1 |
|
Gas |
2 |
|
Water |
3 |
|
Non-GIS |
4 |
The following fields have domains associated with them:
|
Field |
Domain |
|---|---|
|
LABOR_TYPE |
EDM_LaborType |
|
SOIL_CONDITION |
EDM_SoilCondition |
|
TRAFFIC_CONDITION |
EDM_TrafficCondition |
|
NETWORK_STATUS |
EDM_NetworkStatus |
The domains are defined as follows:
EDM_LaborType
|
Code |
Value |
|---|---|
|
0 |
Internal |
|
1 |
Contractor |
EDM_SoilCondition
|
Code |
Value |
|---|---|
|
0 |
Soft Soil |
|
1 |
Firm Soil |
|
2 |
Hard Soil |
EDM_TrafficCondition
|
Code |
Value |
|---|---|
|
0 |
No Traffic |
|
1 |
Light Traffic |
|
2 |
Medium Traffic |
|
3 |
High Traffic |
EDM_NetworkStatus
|
Code |
Value |
|---|---|
|
0 |
Not In Service |
|
1 |
In Service |
The Labor_Type, Soil_Condition, Traffic_Condition, and Network_Status fields must have a short integer data type because they appear on the Site Conditions tab in Workflow Manager. All fields on this tab must utilize a domain.
EDM_DESIGN
This table manages the extended data for a design. No field model names exist. This table uses the same domains as the EDM_COMPATIBLEUNIT table. This table does not have subtypes.
EDM_WORKLOCATION
This table manages the extended data for a work location. No field model names exist. This table uses the same domains as the EDM_COMPATIBLEUNIT table. This table does not have subtypes.
EDM_WORKREQUEST
This table manages the extended data for the work request feature. No field model names exist. This table does not have subtypes. The WORKREQUEST_TYPE field has the EDM_WorkRequestType domain associated with it.
The EDM_WorkRequestType domain is defined as follows:
|
Code |
Value |
|---|---|
|
0 |
None |
|
1 |
Residential |
|
2 |
Commercial |
|
3 |
Irrigation |
|
4 |
Industrial |