Create Classes
Create the following feature and object classes in the UFM dataset. If you are using the sample data, these may already exist in a separate dataset. Feel free to add them to a new dataset or to an existing dataset. These features do not participate in a geometric network.
Duct feature class: This feature class represents the point at which items in an underground distribution system enter the manhole. Ducts are open connections to the conduit system.
Users must not modify the DuctPosition value. This value is maintained by ArcFM. Set the Editable and Visible field properties on this field to No (Field Info tab on the ArcFM Properties Manager).
Shape: Polygon
|
Field Name |
Data Type |
Domain |
|---|---|---|
|
HasSubducts |
long integer |
Yes/No Indicator |
|
PhaseDesignation |
long integer |
Phase Designation |
|
DuctPosition |
long integer |
|
|
DuctName |
text (length=50) |
|
|
DuctSize |
text (length=50) |
ULS Size |
|
Available |
long integer |
Yes/No Indicator |
|
Occupied |
long integer |
Yes/No Indicator |
|
Material |
text (length=50) |
ULS Material Duct Bank |
DuctAnnotation feature class: This annotation feature class provides general notes annotation for duct position.
When creating the DuctAnnotation class, link the annotation to the Duct feature class.
Type: ArcFM Annotation Feature
Reference Scale: 1:30 (This is the scale at which the label’s font size appears “normal.” This annotation is visible when extremely zoomed in; thus, this scale is appropriate).
Fields: No additional required fields.
DuctBank feature class: This feature class contains the ducts.
Shape: polygon
|
Field Name |
Data Type |
|---|---|
|
FacilityID |
text (length=20) |
|
RelConduitSystemObjectId |
long integer |
DuctBankAnchor feature class: Optional. This point feature class is used to store duct banks as composite favorites. It is necessary only if you wish to create composite favorites using duct banks.
Shape: point
|
Field Name |
Data Type |
|---|---|
|
SymbolRotation |
double |
DuctConnector feature class: This linear class provides the logical routing of a conductor from one duct to another through a manhole.
Shape: line
|
Field Name |
Data Type |
Domain |
|---|---|---|
|
PhaseDesignation |
long integer |
Phase Designation |
DuctDefinition object class: This table defines the attributes that are stored for each duct (conduit). Any number of fields may be added to this table, but the following is required for UFM. This table is created during the basic Conduit Manager configuration.
|
Field |
Data Type |
Domain |
|---|---|---|
|
DuctSize |
text (length=255) |
ULS Size |
DuctNoteAnno feature class: This annotation feature class provides general notes annotation for ducts.
When creating the DuctNoteAnno class, DO NOT link the annotation to any other feature class.
Type: ArcFM Annotation Feature
Reference Scale: 1:25 (This is the scale at which the label’s font size appears “normal.” This annotation is visible when extremely zoomed in; thus, this scale is appropriate).
Fields: No additional required fields.
Splice feature class: OPTIONAL. This class represents a splice and is not required.
Shape: point
Fields: No additional required fields.
UFMAnchor feature class: This feature class is necessary for saving a butterfly diagram as a composite favorite.
Shape: point
|
Field Name |
Data Type |
|---|---|
|
SymbolRotation |
double |
UFMFloor feature class: This class represents the floor of a manhole.
Shape: polygon
|
Field Name |
Data Type |
|---|---|
|
FacilityID |
text (length=50) |
UFMInsetFrameSource feature class: You may create this polygon feature class or use an existing InsetFrameSource feature class (e.g., ElectricInsetFrameSource).
Shape: polygon
|
Field Name |
Data Type |
|---|---|
|
Title |
text (length=50) |
UFMWall feature class: This polygon class represents the walls of the manhole.
Shape: polygon
|
Field Name |
Data Type |
|---|---|
|
FacilityID |
text (length=50) |
UFMWallDimensioning feature class: This polygon class is used to show annotation that displays width and height values of underground facility walls. This class is optional.
Type: ArcFM Dimension Feature (ArcFM autoupdaters will not fire on Esri Dimension Features)
Set the following options while creating the dimension feature.
Reference Scale: 1:50 (This is the scale at which the label’s font size appears “normal.” This annotation is visible when extremely zoomed in; thus, this scale is appropriate).
Default Style: "I would like to create my own style", then click New Style button
Style Properties: Select Fit tab and select the following options: Do not adjust arrows, Do not adjust text. Unselect the following: Extend dimension line to length of text. Click OK
Accept remaining default values.
Fields: No additional required fields.
UndergroundStructure feature class: This class represents the manhole. It may already exist in your dataset, but the following fields must be added.
Shape: point
|
Field Name |
Data Type |
Domain |
|---|---|---|
|
SubtypeCD |
long integer |
|
|
FacilityID |
text (length=50) |
|
|
Material |
text (length=20) |
|
|
StructureSize |
text (length=20) |
|
|
StructureType |
text (length=20) |
|
|
Manufacturer |
text (length=20) |
|
|
Model |
text (length=20) |
|
|
Comments |
text (length=100) |
|
|
WorkOrderID |
text (length=20) |
|
|
InstallationDate |
date |
|
|
SymbolRotation |
double |
|
|
Enabled |
short integer |
|
|
FacilityDiagram |
long integer |
Yes/No Indicator |