Add Fields
You may need to add fields to the following feature classes. You may use any names for your fields. The names shown are those used in the sample data.
wClear Well
This feature class isn't currently used by water tracing. However, it is part of the network and requires the WaterTraceWeight field.
|
Field |
Data Type |
|---|---|
|
WaterTraceWeight |
long integer |
wControl Valve
|
Field |
Data Type |
Domain |
|---|---|---|
|
BondedIndicator |
text (length=5) |
Yes/No Indicator |
|
CPSystemStatus |
long integer |
CPSystemStatus |
|
EmerIsolationSysStatus |
text (length=20) |
|
|
InsulatedIndicator |
text (length=5) |
Yes/No Indicator |
|
Material |
text (length=5) |
Water Line Material |
|
NormalPosition |
long integer |
Normal Position |
|
OperatingClassification |
text (length=5) |
Operating Classification |
|
Status |
text (length=5) |
Station Status |
|
WaterPressureSystemStatus |
text (length=20) |
GasWaterSystemStatus - String |
|
WaterSystemStatus |
text (length=20) |
GasWaterSystemStatus - String |
|
WaterTraceWeight |
long integer |
wFitting
|
Field |
Data Type |
Domain |
|---|---|---|
|
BondedIndicator |
text (length=5) |
Yes/No Indicator |
|
CPSystemStatus |
long integer |
CPSystemStatus |
|
EmerIsolationSysStatus |
text (length=20) |
|
|
InsulatedIndicator |
text (length=5) |
Yes/No Indicator |
|
Material |
text (length=5) |
Water Line Material |
|
NormalPosition |
long integer |
Normal Position |
|
WaterPressureSystemStatus |
text (length=20) |
GasWaterSystemStatus - String |
|
WaterSystemStatus |
text (length=20) |
GasWaterSystemStatus - String |
|
WaterTraceWeight |
long integer |
wGravity Pressure Main
|
Field |
Data Type |
Domain |
|---|---|---|
|
BondedIndicator |
text (length=20) |
Yes/No Indicator |
|
CPSystemObjectID |
long integer |
|
|
CPSystemStatus |
long integer |
CPSystemStatus |
|
InsulatedIndicator |
text (length=5) |
Yes/No Indicator |
|
Material |
text (length=5) |
Water Line Material |
|
MeasuredLength |
double |
|
|
PipeStatusIndicator |
long integer |
Normal Position |
|
PipeType |
text (length=50) |
Pipe Type |
|
OperatingPressure |
double |
|
|
Status |
text (length=5) |
Station Status |
|
WaterTraceWeight |
long integer |
wHydrant
This feature class isn't currently used by water tracing. However, it is part of the network and requires the WaterTraceWeight field.
|
Field |
Data Type |
|---|---|
|
WaterTraceWeight |
long integer |
wLateral Point
This feature class isn't currently used by water tracing. However, it is part of the network and requires the WaterTraceWeight field.
|
Field |
Data Type |
|---|---|
|
WaterTraceWeight |
long integer |
wLateral Service
|
Field |
Data Type |
Domain |
|---|---|---|
|
BondedIndicator |
text (length=5) |
Yes/No Indicator |
|
CPSystemObjectID |
long integer |
|
|
CPSystemStatus |
long integer |
CPSystemStatus |
|
InsulatedIndicator |
text (length=5) |
Yes/No Indicator |
|
Material |
text (length=5) |
Water Line Material |
|
MeasuredLength |
double |
|
|
OperatingPressure |
double |
|
|
Status |
text (length=5) |
Station Status |
|
WaterTraceWeight |
long integer |
wManhole
This feature class isn't currently used by water tracing. However, it is part of the network and requires the WaterTraceWeight field.
|
Field |
Data Type |
|---|---|
|
WaterTraceWeight |
long integer |
wMeter
This feature class isn't currently used by water tracing. However, it is part of the network and requires the WaterTraceWeight field.
|
Field |
Data Type |
|---|---|
|
WaterTraceWeight |
long integer |
wNetwork Structure
|
Field |
Data Type |
Domain |
|---|---|---|
|
EmerIsolationSysStatus |
text (length=20) |
|
|
Status |
text (length=5) |
Station Status |
|
WaterPressureSystemStatus |
text (length=20) |
GasWaterSystemStatus - String |
|
WaterSystemStatus |
text (length=20) |
GasWaterSystemStatus - String |
|
WaterTraceWeight |
long integer |
wPump
This feature class isn't currently used by water tracing. However, it is part of the network and requires the WaterTraceWeight field.
|
Field |
Data Type |
|---|---|
|
WaterTraceWeight |
long integer |
wPumpPressureMain
|
Field |
Data Type |
Domain |
|---|---|---|
|
BondedIndicator |
text (length=5) |
Yes/No Indicator |
|
CPSystemObjectID |
long integer |
|
|
CPSystemStatus |
long integer |
CPSystemStatus |
|
InsulatedIndicator |
text (length=5) |
Yes/No Indicator |
|
Material |
text (length=5) |
Water Line Material |
|
MeasuredLength |
double |
|
|
OperatingPressure |
double |
|
|
PipeStatusIndicator |
long integer |
Normal Position |
|
PipeType |
text (length=5) |
Pipe Type |
|
Status |
text (length=5) |
Station Status |
|
WaterTraceWeight |
long integer |
wPumpStation
You may create a feature class that acts as a pressure system barrier. You may also choose to use an existing feature class to serve as a barrier (e.g., Pump). The feature class must contain the following fields with the listed data type.
|
Field |
Data Type |
Domain |
|---|---|---|
|
CPSystemStatus |
long integer |
CPSystemStatus |
|
EmerIsolationStatus |
text (length=20) |
|
|
InletPressure |
long integer |
|
|
OutletPressure |
long integer |
|
|
WaterPressureSystemStatus |
text (length=20) |
GasWaterSystemStatus - String |
|
WaterSystemStatus |
text (length=20) |
GasWaterSystemStatus - String |
|
WaterTraceWeight |
long integer |
wSampling Station
This feature class isn't currently used by water tracing. However, it is part of the network and requires the WaterTraceWeight field.
|
Field |
Data Type |
|---|---|
|
WaterTraceWeight |
long integer |
wSystem Valve
|
Field |
Data Type |
Domain |
|---|---|---|
|
BondedIndicator |
text (length=5) |
Yes/No Indicator |
|
CPSystemStatus |
long integer |
CPSystemStatus |
|
EmerIsolationSysStatus |
text (length=20) |
|
|
InsulatedIndicator |
text (length=5) |
Yes/No Indicator |
|
Material |
text (length=5) |
Water Line Material |
|
NormalPosition |
long integer |
Normal Position |
|
OperatingClassification |
text (length=5) |
Operating Classification |
|
Status |
text (length=5) |
Station Status |
|
WaterPressureSystemStatus |
text (length=20) |
GasWaterSystemStatus - String |
|
WaterSystemStatus |
text (length=20) |
GasWaterSystemStatus - String |
|
WaterTraceWeight |
long integer |