Create Domain
Create the following domains. These may have been created during configuration of another ArcFM Solution tool. The coded values displayed are as they appear in the sample data. They may vary to suit your business needs.
Phase Designation
ArcFM requires that a phase be represented with one character. The domain description of a three-phase conductor has three letters or numbers (e.g., ABC or 123). However, the coded domain values must be single digits. The Minerville sample database uses integers 1 through 7 to describe the combination of phases as shown below.
Field type: Long integer
Domain type: Coded Values
|
Code |
Description |
|---|---|
|
1 |
C |
|
2 |
B |
|
3 |
BC |
|
4 |
A |
|
5 |
AC |
|
6 |
AB |
|
7 |
ABC |
ULS Material Duct Bank
Field type: Text
Domain type: Coded Values
|
Code |
Description |
|---|---|
|
FIB |
Fiber |
|
STL |
Steel |
|
WOD |
Wood |
|
OTH |
Other |
|
UNK |
Unknown |
|
PVC |
PVC |
ULS Size
This domain holds the various duct sizes. The following values are as they appear in the sample data. You may edit these values to reflect your business standards.
Field type: Text
Domain type: Coded Values
|
Code |
Description |
|---|---|
|
2 |
2" |
|
5 |
5" |
|
10 |
10" |
|
4 |
4" |
|
6 |
6" |
Yes/No Indicator
Field type: Long integer
Domain type: Coded Values
|
Code |
Description |
|---|---|
|
0 |
No |
|
1 |
Yes |