Attribute Editor Options

The Attribute Editor tab in ArcFM Options allows you to modify various settings for the Attribute Editor.

General

Enable automatic tab activation: This option changes the tab on the Attribute Editor as selections on the table of contents tabs change. For example, if the QA/QC tab is displayed on the Attribute Editor, and you choose to send a feature to the Targets tab from the Features tab, the Attribute Editor will automatically display the Targets tab.

Selection Tab

You may determine the order in which features appear on the Selection tab. Choose from drawing order or alphabetical order. Selection Tab settings also apply to the Identify Tool.

The Automatically Expand Selection Tab option expands and selects the top node in the list when features are added to the Selection tab of the Attribute Editor.

  • Never: When features are added to the Selection tab, they will remain collapsed until the user expands them.

  • When a single feature is selected: When a single feature is added to the Selection tab (or multiple features in the same feature class), it will be expanded and selected so its attributes are shown in the Attribute Editor grid.

  • Always: The top feature in the list will always be expanded and selected regardless of the number of features selected.

QA/QC Tab

QA/QC Tab options let you choose one of two different ways to display the QA validation results: all selected items or only invalid items. Select "Keep current items" to list all features whether valid or invalid or select "Keep only invalid items" to list only those features with errors.

Targets Tab

Select the "Allow multiple items when using Features tab" checkbox to append features to the Targets tab list. The Targets tab will not be emptied until the user chooses to clear it using the Remove All utility tool. If this checkbox is not selected, the Targets tab will be cleared before each feature is added. This ensures that only the feature being placed will appear in the Targets tab.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?