De-Energized Features

Generally, electrical features that remain de-energized in a normal switching state indicate a data problem, usually in the form of a switchable device that is incorrectly attributed as "open" on one or more phases. This search allows you to locate any de-energized features in the network.

  1. Select the Locate Lines Only checkbox to view only conductor features.
  2. Choose a Substation.
  3. Select a feeder from the grid.
  4. Click Close.
  5. Press Enter or click Find in the ArcFM Locator window to perform the search. Click the Stop button if you want to end the search before it is complete.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?