Copy

Use Copy to move features to the clipboard. You can paste copied features into a Favorites Category on the Features tab (during an editing session). The Copy tool is available regardless of whether an Edit session is started or not. You MUST have an Edit session started in order to use the Paste utility.

  1. Right-click a feature in Attribute Editor.
  2. Select Copy from the Utilities menu.
  3. Right-click a User Favorites on the Features tab.
  4. Select Paste to add the copied feature.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?