Tie Devices and Terminal Devices

Tie Devices are switchable devices set in an open state and that can be energized from two different sources. A Terminal Device is any switchable device that prevents electrical power from reaching some features because of its "open" status on one or more phases.

The Feeder/Tie locator allows you to locate all tie and/or terminal devices and filter the resulting set into those devices associated with a given feeder or group of feeders.

  1. Choose a Substation.
  2. Select a feeder from the grid.
  3. Click Close.
  4. Press Enter or click Find in the ArcFM Locator window to perform the search. Click the Stop button if you want to end the search before it is complete.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?