Explore Pane

Use the Explore pane in the Compatible Unit Filter to create and organize palettes and searches. This section also offers topics that discuss creating and editing Palettes and Searches

Expose or hide the Explore pane using the show/hide button above the Filters section.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?