Work Function Tool Overview

The Work Function Tool (WFT) is used for removing, replacing, and upgrading features as part of a design scenario. It also provides in-place editing of features and site condition data, and allows CU assignment on multiple features simultaneously. Users can also use Favorites to achieve their Design goals. We have included a use case to illustrate how a favorite can be used in the workflow. You must have a design open to use the Work Function Tool. You may use Workflow Manager to open and manage designs.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?