Highlight Conduit

The Highlight Conduit option is a tool in the right-click menu for the Selection tab of Attribute Editor. It highlights the associated conduit of a selected duct feature and helps identify the correct associated conduit. This is particularly helpful when looking at a wall with several conduit present. This tool is available only when one duct feature is selected at a time.

To highlight associated conduit, right-click on a selected duct feature in the Selection tab of Attribute Editor, then select Highlight Conduit from the context menu.

TIP: You can also use the hot Key is Ctrl+I to highlight the associated conduit for the selected duct feature.

The associated conduit highlights on the map.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?