ArcFM Inset Frames

The ArcFM Inset Frames tool allows you to display specific features within your current view individually in separate windows. For example, you can depict each switching facility in the Switching Facility layer in its own inset frame. These individual inset frames are shown in a window.

Inset frames are available in both ArcFM and ArcFM Viewer. Some functionality requires editing and is not available in ArcFM Viewer. Functionality available in ArcFM (and not in ArcFM Viewer) is noted in each appropriate topic.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?