Basic Redliner

Due to so many links to topics everywhere, and so many repeat, duplicate topics, I am placing this comment in topics I’ve already fixed that I know are linked to a bunch or that I know I have seen a bunch and that I want to ensure aren’t duplicates or see if I can reuse something {this is the case for Enable Dir Browsing and Configure Bits}. AMS 12/2018

Basic Redliner enhances the view-only functionality with the ability to place redline graphics. These graphics may be sent between the enterprise and field.

Required Licenses in the Field: Redliner Extension and ArcFM Viewer for ArcGIS Engine or ArcFM Viewer

Field Databases: Backdrop, Login (optional), Process Framework (e.g., Session Manager or Workflow Manager)

Perform the steps in this section to configure Basic Redliner.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?