Process Framework Database (Send/Receive)

This replica moves sessions and designs between the field machines and the Enterprise. You can choose to configure a Process Framework replica to do this, or you can use the Mobile Synchronizer instead.

A copy of the field Process Framework database (e.g., fieldsessionmanager.mdb, fieldworkflowmanager.mdb) should reside on the administrator machine. When you're ready to distribute to all client machines, copy it to the same directory (e.g., C:\ReplicationField\ProcessFramework).

To configure the Process Framework replica, follow the steps outlined on the following pages.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?