Upgrade Workflow Manager to 9.2.1

Use these upgrade instructions if you are:

  • Using a version of Workflow Manager older than 9.2.1

  • Upgrading to a version of Workflow Manager that is 9.2.1 or higher

These instructions are intended for GIS administrators who currently are in production with Workflow Manager and who want to upgrade to the most recent release of the ArcFM Solution. This document does not apply if you are not currently using Workflow Manager and will be implementing it with the most recent version of the ArcFM Solution (i.e., you are new to ArcFM and are starting with the most recent release). If this is the case, refer to Set Up Workflow Manager.

If you are upgrading your Process Framework, you may also need to use the Process Framework Database Upgrade tool.

Upgrade to 9.2.1

The following changes should be made to the Workflow Manager field database (e.g., Field WorkflowManager.mdb) if you wish to use ArcFM Redliner to create and edit designs in the field. If you are not using Redliner or do not wish to use designs with Redliner, the upgrades on this page are not necessary. No changes are required for the enterprise Workflow Manager database when upgrading to 9.2.1.

Tasks

You will need to create the following task using the Process Framework Administration Tool. The Task Name must appear exactly as shown in bold below.

  • Open Redline Design

Node Type: design

Assign Subtasks: (in order as shown)

  • Open Redline Session

  • Send Design

Node Type: design

Assign Subtasks: (in order as shown)

  • Send Design

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?